STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

I have installed the latest (en.stm32cubeprog_v2-3-0) version in Windows 10 64 bit PC. After installation, the first startup icon with spinner only comes up , closes and does not run. As far as googled and found online, it is java versioning issue.

I have installed the latest (en.stm32cubeprog_v2-3-0) version in Windows 10 64 bit PC.After installation, the first startup icon with spinner only comes up , closes and does not run.As far as googled and found online, it is java versioning issue. Thi...

PPK by Associate II
  • 1028 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer gives me an error

I'm trying to program STM32L031 microcontroller using STLINK but STM32CubeProgrammer gives me the following error:Error: No STM32 target found!These are the conditions:1) The hardware is correctly connected because the STM32CubeIde emulates correctly...

PNenn.1 by Associate
  • 1083 Views
  • 1 replies
  • 0 kudos

Resolved! STM32Cube Programmer API USB Example error

Hello,I put my STM32H743XI in Bootloader mode and launch STM32Cube Programmer USB example on VS and got : I have two question :Where does this error comes from and how to fix it ?Can I skip option bytes programming and still flash my MCU ?Regards

0693W0000059bznQAA.png

Resolved! STM32CubeProgrammer Install/Uninstall issues. I can't uninstall the previous version of the Programmer. The newly installed version won't run.

Trying to uninstall the previous version, I get: "Windows cannot find C\Program Files (x86)\Java\jre1.8.0_251\bin\javaw.exe. Trying to run the newly installed Programmer, I get "CubeProgrammer_API or one its dependencies is missing. Please try reinst...

Resolved! Error to connect to target STM32H747I-DISCO

I try to connect to target STM32H747I-DISCO but show this message:08:58:19 : ST-LINK SN : 004800413137510D3938353808:58:19 : ST-LINK FW : V3J3M208:58:19 : Voltage : 3.27V08:58:19 : No STM32 target found!08:58:20 : ST-LINK SN : 004800413137510D393835...

Programming STM32F405 in bootloader mode via stm32cube programmer command line interface at the address 0x08008000, the programming processes completes successfully but the controller does nothing afterwards I don't understand why?

I am student developing an app that uses the STM32CubeProgrammer command line interface executable to program STM32F405.The controller works as excepted if it is programmed at the address 0x08000000.but sometimes the programming processes fails or st...