STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

ST-LINK_gdbserver and load to Ram

It seem that ST-LINK_gdbserver does not implement load to run.(gdb) tar ext :61234 Remote debugging using :61234 0x0800004e in ?? () (gdb) info mem Using memory regions provided by the target. Num Enb Low Addr High Addr Attrs 0 y 0x00000000 0...

Resolved! How to wire stm32c031f6 OTP

HI: I want to write the board SN, REV, TIME to STM32C031F6 OTP area 0x1FFF7000~0x1FFF705F, which is almost 96bytes to write, from the stm32cubeprogrammer manual -W64 command can to write, but is needs to be repeated 6 times, right?Also from the manua...

RJ3 by Associate
  • 1344 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeProgrammer

I am trying to program a chip using an STLINK V2. I am using only SWDIO, SWCLK, and ground, and I am powering the chip with 3.3 V. When I try to connect using STM32CubeProgrammer, it does not connect. Am I missing something?

tomm5771 by Associate III
  • 4936 Views
  • 6 replies
  • 1 kudos

Create a dual core project from compiled binary file

Hello,The main purpose of the question is to avoid giving source code and give binary file instead.For example, I generate a compiled binary file from a nucleo project (STM32H743ZI2) for the M7 core.Then I want to create a new dual core project (STM3...

Kévin by Associate III
  • 2122 Views
  • 2 replies
  • 3 kudos

STM32G0 External Loader for I2C eeprom

Hi,I try to make a external loader for STM32G030. I was implemented function MassErase(), Write(), Read(), Init()...First I test function on "flash" version and everything work. But when I try using it in STM32CubeProgrammer the Write function not wo...

arekj by Associate II
  • 2758 Views
  • 4 replies
  • 0 kudos