STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32H7B3i-DK Error: No STM32 target found

The STMCubeProgrammer would no longer connect to my target. I was able to create a simple test program with Keil toolchain and step through the code and suddenly I noticed that the board stopped responding.I then tried connecting to the board with ST...

onio by Senior
  • 4101 Views
  • 9 replies
  • 2 kudos

RDP Level 1->0: Can ANYTHING survive ??

I am using STMCubeProgrammer in USB DFU mode to change from RDP Level 1 to 0 (using command line -rdu option). This nukes (mass erases) all flash and all "backup SRAM" (according to datasheet).My product has a couple of bytes of custom config data ...

Goof Ball by Associate III
  • 1509 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer gives error: "No STM32 target found!"

I have a custom board with one STM32H743ZIT6 (“Control MCU�?) and six STM32H7V43VIT6 MCUs. The idea, eventually, is for the Control MCU to reset the six slave MCUs.Right now, after an initial flashing of the slaves with a “bring up�? blinky program t...

APagl by Associate III
  • 2141 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer fails to program STM32L0s MCU when the size of the file to program is not a multiple of 8.

Hi,I am experiencing a problem with STM32CubeProgrammer: it fails to program STM32L0s MCU when the size of the file to program is not a multiple of 8.In the attached zip file, there are 2 .bin files containing 16 bytes of zeros (working.bin), and 20 ...

olivier by Associate III
  • 4138 Views
  • 8 replies
  • 0 kudos

How to update the FW by CubeProgrammer via USART?

I want to update the FW to H7 MCU via its USART by embedded bootloader. It seems need to control the BOOT0 pin and nRST pin when the MCU is in normal running. By CubeProg tool, how to control above 2 pins by PC? Usually, I will build a USB to UART br...

JZou.2 by Associate II
  • 2750 Views
  • 8 replies
  • 0 kudos