STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! FDCAN Bootloader in STM32G474RCT6

I am using STM32G474RCT6 microcontroller, I want perform firmware upgrade through CAN communication. But my controller doesn't provide the feature of Firmware upgrade through CAN communication.is there any possibility to use CAN communication for fir...

Sri_Nishanth_0-1701082492037.png

Resolved! flash a program on STM32N6570DK

  Hi, I created a project on the STM32N6570DK and I only have the project "in (STM32CubeIde)", I don't have the FSBL and the Appli. How do I flash my firmware? I tried to use the fsbl provided by the official ST repository, namely "ai_fsbl.hex", but ...

elena01 by Associate
  • 618 Views
  • 2 replies
  • 1 kudos

Resolved! using SEGGER JLINK with cubeprogrammerCLI

I'm trying to connect my STM32H743IGTX controller with JLINK using cubeprogrammerCLI. I am able to connect jlink with cubeprogrammer gui and able to flash. but when i tried using CLI it shows-----------------------------------------------------------...

Resolved! libusb warnings

I keep getting warnings when using STM32CubeProgrammer_CLI that usb devices are still referenced: libusb: warning [libusb_exit] device x.x still referenced. This is a bit annoying.-------------------------------------------------------------------STM...

Arno1 by Senior
  • 3373 Views
  • 5 replies
  • 1 kudos