User Activity

Hello,I need guidance to create a very simple AI project using CubeIDE (CubeMX) and Neural-ART runtime. I can use all the example projects successfully but failed to create one from scratch till now. I faced no challenge earlier when using H7 for my ...
Hello,I am facing some strange errors when trying to analyze any TFLite model. The errors are occurring in the following situations:Situation 1: STM32Cube.AI MCU RuntimeWhen analyzing a TFLite model, it fails and shows an error message: "TOOL ERROR: ...
Hi, I can't erase the external flash or write a new binary on my STM32N6570-DK board. My problem is similar to this post: STM32N6570-DK: Cannot erase external Flash. But the solution in that post didn't work for me.I have tried using two external loa...
I am using X-CUBE-AI 9.0.0 in my project and need to run a quantized mobilenet_v2.0.35 model (.tflite). The model takes 4*56*56*3 (Batch * width * height * channel) input, but I am unable to find a way to run it with that input shape. The generated c...
Kudos from
Kudos given to