Skip to main content
Sungjae Kim
Associate II
January 16, 2025
Solved

No STM32 target found - STM32G030K6T6

  • January 16, 2025
  • 4 replies
  • 2657 views

Hi, I'm making a board for UART and I2C communication.

Please refer to the schematic below;

 

SungjaeKim_0-1737011644144.png

 

I put 5V External power supply at VBUS,

and connects SWDIO, SWCLK, NRST, 3V3, GND to the STLINK V3 Minie.

 

However it shows "No STM32 target found" message on STM32CubeProgrammer when I clicked "Connect" button.

Since the "Target voltage" shows 3.31V, I think there is no power problem.

Is there something that I missing?

Please let me know.

Thank you.

This topic has been closed for replies.
Best answer by STTwo-32

Hello @Sungjae Kim 

What I can see is that you are using PA13 as SWCLK and PA14-BOOT0 as SWDIO. But according to the Table 12 of the DS12991 Rev4 , you should be using PA13 as SWDIO and PA14-BOOT0 as SWCLK:

STTwo32_0-1737013121419.png

 

Best Regards.

STTwo-32

 

4 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
January 16, 2025

Hello @Sungjae Kim 

What I can see is that you are using PA13 as SWCLK and PA14-BOOT0 as SWDIO. But according to the Table 12 of the DS12991 Rev4 , you should be using PA13 as SWDIO and PA14-BOOT0 as SWCLK:

STTwo32_0-1737013121419.png

 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Sungjae Kim
Associate II
January 16, 2025

STTwo-32, Thank you for prompt reply and catching my mistake.

I have twisted SWCLK and SWDIO, now it recognized successfully.

Thank you and have a nice day :)

Peter BENSCH
ST Technical Moderator
January 16, 2025

@Sungjae Kim And please do yourself a favor and connect a 100nF from pin NRST to GND, which guarantees a clean reset at power-up.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.