STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Reset the discovery kit to the defalut setting

Hi,I would like to know how to reset the discovery kit to the default setting?And how do I know about the current setting (write protection is enabled/disabled)in the discovery kit?The reason is that,I suddenly can't run anything on my board(even jus...

0693W000006HeWyQAK.png
LChiu.2 by Associate
  • 1448 Views
  • 2 replies
  • 0 kudos

Resolved! Hi. I have been trying to flash an STM32L152RD (STM32L1xxxD) using the CUBE programmer through the USART2 and it never connects (Timeout error occured while waiting for acknowledgement). I have used the software method of branching into the bootloader

Because I do not have access to the BOOT0 pin (custom board, not eval board) I have used the software method of branching into the bootloader : https://stm32f4-discovery.net/2017/04/tutorial-jump-system-memory-software-stm32/I have adpted this code f...

JBaue.1 by Associate II
  • 6997 Views
  • 10 replies
  • 0 kudos

The difference between saving .bin and .elf files

I'm working with STM32H743 and W25Q128 external flash drive. I am trying to develop external loader. When I test with STM32CubeProgrammer and .bin files, everything works fine, writes to 0x90000000 address, verifies and reads OK. When I try to upload...

ISzum by Associate II
  • 7878 Views
  • 6 replies
  • 0 kudos

Error downloading Thread_SED_Coap_FreeRTOS

Hello thereI am using the official engineering code Thread_SED_Coap_FreeRTOS. When downloading with STM32CubeProgrammer, the error message connection to device0x495 is lost appears. At this time, the program should fail to download because the LED1, ...

0693W000006FJo9QAG.jpg 0693W000006FJqoQAG.jpg 0693W000006FJp2QAG.jpg
ZB.1 by Associate II
  • 2447 Views
  • 5 replies
  • 0 kudos

Resolved! cannot launch STM32CubeProgrammer

Hi,I just bought the STM32MP157F-EV1 and was trying to get it started.I tried to followed the manual written in the website and I thought I have completed step 4 and step 5 in the manual.However, when I tried to populate the SDCard, I realize that I ...

0693W000006Gpd6QAC.png 0693W000006GperQAC.png 0693W000006GpfLQAS.png
devinahw by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

Resolved! SWO viewer for STM32CubeProgrammer?

Hi,We're currently using the SWO viewer in the old ST-Link Utility in Windows.However, this is a bit inconvenient for us because our main development is in Linux. Is SWO support planned for STM32CubeProgrammer? Even just STM32Programmer_CLI SWO suppo...