cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer v2.21 released

Aziz BRIGUI
ST Employee

We are pleased to announce that STM32CubeProgrammer 2.21 is available

What is new in 2.21:

• Support for the STM32WL3Rxx microcontrollers:

        – Internal memory programming
        – Option byte and OTP programming
        – PKCS#11
        – Firmware authentication

• STM32MP21x microprocessors: SSP support on Linux®
• STM32WBA6xxG microcontrollers: Support for 1-Mbyte flash memory size
• Support for new devices in the STM32C0 series: STM32C011xx, STM32C031xx, STM32C051xx, STM32C071xx, STM32C091xx, and STM32C092xx microcontrollers

• Support for the factory reset of option bytes:
        – STM32WBA5xxx and STM32WBA6xxx microcontrollers

        – STM32U375/385 microcontrollers
• Dynamic upgrade of components
• Support for SWD multi-drop
• Fast read new CLI command

Main fixed issues in 2.21:

Refer to the STM32CubeProgrammer wiki at:

STM32CubeProgrammer errata 2.21.x - stm32mcu

Known problems and limitations in 2.21:

Refer to the STM32CubeProgrammer wiki at:

STM32CubeProgrammer errata 2.21.x - stm32mcu

How to get STM32CubeProgrammer 2.21:

  • Under this link
  • Or update your current installation of STM32CubeProgrammer using: Help > Software update

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0