STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

CubeProgrammer, erm...

Control is confusing. What's wrong with normal menus and tabs? And the worst idea, Save File is a pulldown of the Read button. Took me some time to discover.Please, ditch the "modern feel and look" (and this of course goes also for the web, the forum...

Writing 8-bit data not working correctly in CLI

Writing 8-bit eeprom data with STM32_Programmer_CLI only works when writing to 32-bit aligned addresses i.e. 0x08080000 or 0x08080004 but not with 0x08080001.Example commands:$ ./STM32_Programmer_CLI.exe -c port=SWD -w8 0x08080000 0x10   Downloading ...

internal flash memory not programmed

Hi , i want to program a stm32f030f4p6 mcu with st-link but this problem is appeared for me : when i connect to the mcu i can erase chip easily , but when i program it , the content of flash memory not changed , the value of all blocks in flash memo...

0690X000009YDK3QAO.png

STM32CubeProgrammer not detecting ST-Link devices

I am running Windows 7 and v2.1.0 of the STM32CubeProgrammer. It is unable to find connected ST-Link devices (in this instance, an ST-Link/V2, a Nucleo STM32F411RE, and a Nucleo STM32F303RE).However, if I click the "Firmware Upgrade" button, it is a...

MZimm.13 by Associate
  • 1456 Views
  • 2 replies
  • 0 kudos