STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Boot loader with stm32CubeProgrammer

Thank you for helping.environment:MCU: STM32F769BIProgrammer: stm32CubeProgrammer Ver2.6.0I booted with the BOOT pin of the MCU set to H level and tried to write the hex file by the boot loader using USART1.It's progressing halfway, but I always get ...

Ebun.1 by Senior
  • 2606 Views
  • 5 replies
  • 0 kudos

Resolved! How to Data communicate with the STM32 BOOTLOADER ?

I want to make a Tool like STM32CubeProgrammer using MFC.When I checked the device monitoring, STM32CubeProgrammer was able to communicate 2K at a time.When connected via USB, the device manager shows up as STM32 BOOTLOADER, I am trying to connect th...

JPark.20 by Associate II
  • 1439 Views
  • 2 replies
  • 0 kudos

Resolved! How to write FW to stm32g070 by CubeProgrammer via UART

I want to program the FW via UART.Read and erase function are working fine, but write function is not working with below error message.Anybody has a knowhow about this problem? 14:35:12 : Port configuration: parity = even, baudrate = 115200, data-bit...

EHeo.1 by Associate
  • 1193 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer ZULU8 Jre recommended

STM32CubeProgrammer requires a Java™ Runtime Environment (JRE) to execute and In April 2019, Oracle decided to change their economic model around Java.Since this date the Oracle JVM beyond version 1.8u211 becomes non-free for professional usageFor S...

Unable to run stm32cubeprogrammer due to Java issue

I get the following error when I try to run STM32CubeProgrammer both as admin or non-admin. My system details: Windows 10Java versions : I have tried using cubeprogrammer 2.5 as well as 2.4 and I get the same error in both cases. Please let me know i...

GRang.1 by Associate II
  • 5807 Views
  • 4 replies
  • 0 kudos

Hi, I reacently desgined my first custom STM32 hardware. I am using an STM32L432KCUx controller and the firmware i programmed it with does not seem to be executed.

I use Cube Programmer V2.4 and i am programming the chip using USB DFU mode. Its a simple firmware with a blinking LED to get to know how programming unsing DFU works. I tested the firmware on the NUCLEO L432kc board and there it seems to work fine.T...

DKers.1 by Associate II
  • 2480 Views
  • 7 replies
  • 0 kudos