STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer 2.8.0

New features • Added the support for the STM32U575/585 microcontrollers • Added the support for SFI via the JTAG interface for the STM32U575/585 microcontrollers • Added the support for SFI via the bootloader interface (USB/UART/I2C/SPI) for the STM3...

Resolved! Quadspi image/font data stored wrongly

Board Name : stm32f7 seriesQUADSPI : N25Q128AI am stored imaged data in nor flash, data stored correctly in memory. After i am reset the controller or power on the controller, data will be resetExample :data : 0xD3005600Data stored first time p...

0693W00000FCADOQA5.png 0693W00000FCAEvQAP.png

How to erase external flash from CLI?

I would like to erase the external flash from terminal using STM32_Programmer_CLI.Using the command STM32_Programmer_CLI -c port=SWD freq=4000 mode=UR -el MX25LM51245G_STM32H735G-DK.stldr --erase alldoes not seem to erase the external flash.Giving th...

Arno1 by Senior
  • 1043 Views
  • 1 replies
  • 1 kudos

STM32CubeProgrammer cannot finish installing

I am trying to install STM32CubeProgrammer v2.8.0 on my Windows10 (Home x64) computer. I have updated my Java version to 8.301 (64-bit). However, installation process doesn't go further than Step 7 out of 8. There's no "Next" button or something, b...

RDermenci by Associate II
  • 1181 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H743 .bin file is enormous

Hi !I'm used to working with F4 and F7 devices, and I've always made '.bin' files to distribute the firmware upgrades, which can be flashed via a custom bootloader, directly on the board, from an SD card.With my current project however, on a STM32H74...

TGeof.2 by Associate II
  • 5410 Views
  • 8 replies
  • 0 kudos

Resolved! Meaning of "Value" Field in Option Bytes STM32

I am trying to understand the semantics of the "value" field in the option bytes in Cube Programmer. On my STM32G0 part, the PCROP1A_STRT and PCROP1A_END fields have "value" and "address" fields. What are valid inputs for the "value" field? Thanks!

0693W00000FBwiIQAT.jpg
RKher.1 by Associate III
  • 1186 Views
  • 1 replies
  • 0 kudos

STM32cubeProgrammer 2.8.0 download shutdown

hello, so i use STM32cubeprogrammer, so i want firmware but i cant use this program coz The program is forcibly terminated by connecting the device and pressing Download to upload the firmware file. I don't know why. Does anyone know why this is hap...

Mseon.1 by Associate
  • 1355 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 Programmer CLI hangs on parsing large file

I am trying to program an F4 with an external flash chip in mapped memory mode using the STM32_Programmer_CLI. I use the cli commandSTM32_Programmer_CLI.exe --connect port=SWD mode=UR reset=hwRst -halt --erase all --download <path_to_hex> -el <path>...

GDare.1 by Associate II
  • 7179 Views
  • 14 replies
  • 0 kudos