STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! I can't write to my STM32G03 when connect in Hot plug mode, and I get DEV_TARGET_CMD_ERR whenever I try to connect in Normal mode.

I am trying to directly write to some STM32G03 chips.I have an "STM32G030J6M6" and a "STM32G031F6P6" but I am unable to write to them.I can connect to them, using the CubeProgrammer, but only in "Hot plug" mode, and when I try to write anything, like...

LMeye.1 by Associate III
  • 7265 Views
  • 11 replies
  • 1 kudos

STM32CubeProgrammer is not able to successfully connect to or flash an STM32L471. This is a long-standing problem. I have no problem flashing other STM32L parts such as L051 and I have no problem flashing the L471 using an STLinkv2.

When you place the STM32L471 in DFU mode and attempt to connect via UART, the following is displayed in STM32CubeProgrammer:14:39:27 : STM32CubeProgrammer API v2.5.014:39:28 : Serial Port COM9 is successfully opened.14:39:28 : Port configuration: par...

_dalbert by Associate III
  • 2645 Views
  • 4 replies
  • 1 kudos

Program crash if MCU not powered

I wanted to connect to my STM32 MCU with STM32CubeProgrammer but forgot to power on the board. The programmers (I had 2 boards with 2 STLINK-v3MINIs connected) were detected but when I connected to one, STM32CubeProgrammer crashed. When powered every...

Arno1 by Senior
  • 808 Views
  • 0 replies
  • 1 kudos

AT25SF128A External Flash Loader

Hi, I used MT25QL128 flash memory in my project. This product was obsolute then, I decided to use AT12SF128 flash memory instead of MT25QL128 . Now, I use STM32 Cube Programmer and can not write external memory . Program give "memory edition verifica...

Nbaşa.1 by Associate II
  • 14387 Views
  • 15 replies
  • 0 kudos

Resolved! STM32Cube Programmer

Hi amazing forum.. I am wondering if there is a way to save as HEX file the memory read from the stm32 cube programmer.. I am asking this because I want to check that the bootloader that I am creating is exaclty writing what I expect ...Thanks a lot...

SGasp.1 by Senior
  • 7159 Views
  • 4 replies
  • 1 kudos