STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Unable to connect (& hence flash the firmware) the STM32-Cube-Programmer with STM32-target-board in USB-DFU-mode if loaded firmware is read-protected.

1) I am able to connect the STM32-Cube-Programmer in USB-DFU-mode if existing or loaded firmware in to STM32-target-board is not read-protected.Image-1: Able to connect with target boardImage-2: Able to load firmware in to target board2) I am not abl...

0690X000009Z7piQAC.png 0690X000009Z7qWQAS.png 0690X000009Z7rUQAS.png

Resolved! STM32CubeProgrammer reset not working with RDB=0xBB

If I set read protection (RDP=0xBB) on my STM32H7 MCU, it seems that both software reset and hardware reset commands stop working, e.g. I type:STM32_Programmer_CLI -c port=SWD sn=XXXXXXX reset=HWrst -hardRstand nothing happens. Also, the MCU will not...

sute by Associate III
  • 3229 Views
  • 5 replies
  • 0 kudos

STM32CubeProgrammer 2.11.0 released

New features • Tool updater: can be used to upgrade STM32CubeProg from v2.10.0 to v2.11.0 for all supported operating systems (Windows®, Linux®, and macOS®) • SFI: – SFIx support for STM32U585xx microcontrollers via SWD/JTAG – New SFI/SFIx graphical ...