HiBecause there is not CUBE generated working version for the STM32 H743ZI2 i am using the Web Server Netconn example I noticed the HAL_Delay(1000) is actually 3 seconds.How can it be fixed?Thanks!
HelloCan someone from ST please put here to download a Working example of the ABOVE?There is noting that workingThe web server is CMSIS v1and the cube does not work at all for ethernet!Thanks
I downloaded latest STM32Flash loader for using the UART boot loaderbut it does not select and see the STM32H743Zi Nucleo boardi searched and found that version 2.8 which i am using does not have MAP file for the H7 Series The flash loader do support...
This question was asked but it is now closed , so i want to ask again If some one can share code of how to do sdadc3 for multichannel viaDMA |ISR | interrupts | preferred DMAAll code example shows how to work with single channel.The reason ...