STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STMCube IDE: View generated run command in console

Hello,I am troubleshooting an issue with a provisioning and testing script using the STM32_Programmer_CLI. I get "Failed to erase memory errors" in the CLI but running (as far as I can tell) the same options in CubeIDE does not generate the same erro...

CubeProgrammer couldn't find stm32l476

we are developping sensor reading board which has stm32l412 AND stm32l476RG on it. we could write program to stm32l412 through CubeProgrammer without any problem but we couldn't write to stm32l476. Please addvise possible cause. Both STM32l412/476 ha...

Resolved! CubeProgrammer 2.12 - Operation exceeds memory limits

Hello Everyone,Here is my 512kB STM32L15xxE:     -------------------------------------------------------------------                      STM32CubeProgrammer v2.12.0     -------------------------------------------------------------------USB speed  : ...

0693W00000Y9FcEQAV.png
THein.3 by Associate II
  • 6654 Views
  • 3 replies
  • 0 kudos

STM32CubeProgrammer 2.6.0 released

New features• Added the support for dual-core microcontrollers in the STM32WL Series• Extended the support for the STM32G0 Series to the new STM32G0Bxxx and STM32G0Cxxx microcontrollers• Added SFI support via JTAG/UART/SPI for STM32WL5xxx microcontro...

M1 MacBook Air struggles with STM32CubeProgrammer.

My MacBook Air (M1, 2020) macOS Big Sur version 11.5.1 (20G80) struggles with STM32CubeProgrammer. I deinstalled all my java updates and installed the recommended java version according to this post https://community.st.com/s/question/0D50X0000BmnqrB...

0693W00000D15LXQAZ.png 0693W00000D15MQQAZ.png
OKhal.1 by Associate
  • 3785 Views
  • 3 replies
  • 1 kudos

Resolved! Downloading a ".hex" file in dropbox or onedrive path to mcu forces stm32programmer to quit

OS : windows 10 home 64bit​stm32programmer version : 2.9There is a ".hex" file in the dropbox or onedrive path.Downloading to mcu flash forces stm32programmer to quit. If the ".hex" file is not in the dropbox or onedrive path, it is downloaded normal...

ckim.2390 by Associate II
  • 1875 Views
  • 2 replies
  • 0 kudos