I want to write some data into flash memory on STM32G071 MCU as a part of a project. For that, I am using the function 'HAL_FLASHEx_Erase' to erase the pages before writing. While debugging it's working fine. But when I downloaded the code to MCU and...
Hai, I am working with ST Nucleo H743ZI board for analog-to-digital conversion without CPU intervention between samples, by using DMA in Zephyr platform. Is there any ready-made example for the above, that I can refer?Thank you. Sachin
Hai, I am using ST NUCLEO-H7A3ZI-Q board and I am new it. It worked properly for first one or two times. But now I cant flash code into it, it say "unable to connect to the target". Then I tried STM32CubeProgrammer to connect it and ts connected in '...