cancel
Showing results for 
Search instead for 
Did you mean: 

Error "unable to connect to the target" while flashing to ST NUCLEO-H7A3ZI-Q board.

SJ.7
Associate

Hai, I am using ST NUCLEO-H7A3ZI-Q board and I am new it. It worked properly for first one or two times. But now I cant flash code into it, it say "unable to connect to the target". Then I tried STM32CubeProgrammer to connect it and ts connected in 'Power down' mode. Then I performed Full chip erase. After that the board worked properly.

But the problem arises again when I reconnected the board and I done the full chip erase again.

That is I need to run the full chip erase every time I power the board.

How can I resolve the problem?

Thank you.

Sachin

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Make sure your code sets LDO/SMPS and VOS settings appropriately, and doesn't disable, change or reconfigure the SWD involved pins.

Check SystemClock_Config(), etc, here example for NUCLEO-H7A3ZI-Q from H7 repo

static void SystemClock_Config(void)
{
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 
  /*!< Supply configuration update enable */
  HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY); // << THIS
 
  /* The voltage scaling allows optimizing the power consumption when the device is
  clocked below the maximum system frequency, to update the voltage scaling value
  regarding system frequency refer to product datasheet.
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
 
  while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
 
...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

Make sure your code sets LDO/SMPS and VOS settings appropriately, and doesn't disable, change or reconfigure the SWD involved pins.

Check SystemClock_Config(), etc, here example for NUCLEO-H7A3ZI-Q from H7 repo

static void SystemClock_Config(void)
{
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 
  /*!< Supply configuration update enable */
  HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY); // << THIS
 
  /* The voltage scaling allows optimizing the power consumption when the device is
  clocked below the maximum system frequency, to update the voltage scaling value
  regarding system frequency refer to product datasheet.
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
 
  while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
 
...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MM..1
Chief III

I mean your code put MCU to STOP or any low power mode. This result to unable to connect.

You have two ways out

  1. activate your code from low power before flash
  2. in configuration programming setup Enable debug in low power modes,