STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! How to write EEPROM with STM32CubeProgrammer via USB?

Hi Everyone,I have a STM32L1 connected via USB in DFU-Mode.I'd like to write EEPROM, but trying to do so results in "Memory Limits Error".Using old DfuSe 3.0.6., this is possible... What am I missing? Is CubeProgrammer at all capable of writing EEPRO...

0693W00000Y9TZ0QAN.png
THein.3 by Associate II
  • 2339 Views
  • 3 replies
  • 2 kudos

I wish to store data in the flash memory of my STM32G030C8T6 microcontroller. The issue I am facing is that my data is not being stored in contiguous memory banks, but rather the banks are being skipped, as seen from the image.

I have written a small driver code for the same to store different types of data types to a memory location.The link to my code is: Yadnik1/Eeprom-Emulation-driver-STM32 (github.com) and I have taken reference from here: STM32/FLASH_PROGRAM/F1 SERIES...

0693W00000Y8sbDQAR.png
YBend.1 by Associate III
  • 7231 Views
  • 12 replies
  • 1 kudos

Resolved! STM32F429 IWDG freeze in stop mode

Hi,I'm wondering if it's possible to freeze the IWDG in stop mode for STM32F429. I couldn't find this option in the STM32CubeProgrammer. Not sure if this is feasible.Thanks,

YKuo.1 by Associate II
  • 1507 Views
  • 2 replies
  • 0 kudos

Can external loader running on an STM32F030C8 be run from flash, or must external loaders always run from RAM

I am using an STM32f030C8 with External Flash (W25W128) Via SPI, and want to program the extern flash with sound data using STMcubeprogrammer.I found an excellent article (https://community.st.com/s/article/how-to-add-your-spi-flash-into-the-stm32cub...

RMurt.3 by Associate III
  • 2343 Views
  • 4 replies
  • 1 kudos