STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! mbedTLS version 2.28.2.v2 upgrade on secure boot

I would like to use the mbedTLS version 2.28.2.v2 on the secure boot for stm32h743ii controller. I have downloaded SBSFU v2.6.2 and Built the secure boot binary on top of the example project from H753 2_images_OSC folder. Secure boot is running the t...

mr.1 by Associate III
  • 6632 Views
  • 9 replies
  • 4 kudos

Resolved! SBSFU | 1 Image Download and Decryption

Hello all.Another question regarding SBSFU, this time 1 image version.When we download new image via YMODEM, when does decryption process happen?1. Is new image first downloaded into active image slot and then decrypted?2. Is new image downloaded and...

Resolved! Porting STM32G071 SBSFU to STM32G0B1 issues and queries

Hi Community,I'm porting STM32G071 SBSFU to STM32G0B1RE and Customizing UART to USB CDC.I'm using Nucleo-G0B1RE dev kit and STMCubeIde for development.1. I'm able to build, load, run both STM32G071 SBSFU and UserApp without any changes. but when I ch...

Tarun by Associate III
  • 1761 Views
  • 1 replies
  • 0 kudos

TFM SBSFU_BOOT

Dear Sir.I am trying to work with the examples of TFM_Appication and SBSFU_Boot examples of STMCube_FW_U5_V1.2.0 when compilng I get the error Error: Missing option '-S' / '--slot-size'.postbuild.sh failedmake[1]: *** [makefile:92: post-build] Err...

Resolved! SBSFU 2.6.2 firmware swapping issue

Hi Guys,Ported SBSFU 2.6.2 to STM32G0B1CEU6 (512K FLASH and 64K RAM) based on Nucleo-G071RB example.Modified mapping_fwimg.ld as below: /* Slots must be aligned on 2048 bytes (0x800) */ /* swap (4 kbytes) */ __ICFEDIT_SWAP_start__ = 0x0804...

hw310404 by Associate III
  • 4932 Views
  • 6 replies
  • 2 kudos

Resolved! Error message from debugger back end

Error in final launch sequence:Failed to execute MI command:load D:\\STUSER\\STM32CubeIDE\\workspace_1.13.0\\TEST190923\\Debug\\TEST190923.elfError message from debugger back end:Error finishing flash operation

RKOAS by Associate II
  • 6593 Views
  • 3 replies
  • 0 kudos