STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is Read-out-protection Level1 compatible with IAP ?

Posted on June 25, 2018 at 19:53For a customer I want to set RDP Level1 on STM32F4, and put in first sector a bootloader that manager a jump to DFU for device upgrade.I set the RDP L1 by code at init, and disable it with STMCubeProgrammer.Will the I...

How to enable debug mode for SBSFU?

Posted on February 05, 2018 at 11:12Dear All,I have some questions related to  ♯?:1) How to enable ♯ for ♯ boot-loader and for user application?2) Since I was not able to find an information how to make a ♯ and remove ♯ from the MCU (STM32L476) I wo...

X-CUBE-CRYPTOLIB AES CTR

Posted on May 14, 2018 at 10:07Hi,Does anyone knows how the counter is handled in AES_CTR_Encrypt_Init() / AES_CTR_Encrypt_Append().I suppose it is somewhere in the IV, but the documentation does not talk about it.The examples use an IV initialised ...

STM32F0 read out protection problem

Posted on March 30, 2017 at 10:13Hi,I would like to use a software read protection on STM32F0. I've made such a function:PROTECT_STATUS ReadProtectionConfig(uint8_t ProtectionLevel){ uint8_t status = OK; FLASH_OBProgramInitTypeDef OB_Init; HAL_FLASH...

How to check if the MCU suppot hardware crypto?

Posted on May 12, 2018 at 05:54My device use STM32f437VG (which supports hardware crypto) but sometimes we cannot buy it and use STM32F427VG (which NOT support hardware crypto) instead.So my program have to check if the MCU is 437 or 427 to use prop...

vuahoa07 by Associate II
  • 2503 Views
  • 4 replies
  • 0 kudos

AES128 HW_TIMEOUT error code

Posted on May 11, 2018 at 14:41Hi!I'm struggeling with hardware accelerated aes algorythim. Based on example project I've enabled CRC clock and initilzed the operation, by passing the key (AccHw_AES_CFB_Encrypt_Init(&, , )). After that I'm trying en...

Resolved! STM32F103: unlock RDP without reset

Posted on May 10, 2018 at 00:37Hi, people!how can i reset Read Out Protection on F103 series WITHOUT Power-off and reset??HAL_FLASH_ob_launch --> it is reset (and hold MCU).1. I set the LEVEL from 1 to 0 in subprogramm. All ok. Flash erased, all FF....

STM32F7 Flash Code Readout Protection

Posted on August 07, 2017 at 12:40Are there any examples of enabling (level 1) and disabling code readout protection for stm32f7?I have just tried this on an stm32f767 based on code that worked for stm32f4xx and I seem to have 'bricked' the microcon...

Danish1 by Lead III
  • 16800 Views
  • 4 replies
  • 0 kudos

STM32 Cryptographic library. AES 128bits example fails??

Posted on May 27, 2016 at 13:26Hi,I�m trying to use the �STM32 Cryptographic library package V2.0.6� provided from ST on my STM32F030 device.I�m using IAR Workbench 7.30 and example (AES CTR) compiles without any error.The problem is that data encry...