cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Cryptographic library. AES 128bits example fails??

spankingnator
Associate II
Posted on May 27, 2016 at 13:26

Hi,

I�m trying to use the �STM32 Cryptographic library package V2.0.6� provided from ST on my STM32F030 device.

I�m using IAR Workbench 7.30 and example (AES CTR) compiles without any error.

The problem is that data encrypted doesn�t match with expected data. 

The Key data, IV, plaintext and expected data is being used as example default. I have not touched anything:

const uint8_t Plaintext[64] =

  {

    0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96,

    0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a,

    0xae, 0x2d, 0x8a, 0x57, 0x1e, 0x03, 0xac, 0x9c,

    0x9e, 0xb7, 0x6f, 0xac, 0x45, 0xaf, 0x8e, 0x51,

    0x30, 0xc8, 0x1c, 0x46, 0xa3, 0x5c, 0xe4, 0x11,

    0xe5, 0xfb, 0xc1, 0x19, 0x1a, 0x0a, 0x52, 0xef,

    0xf6, 0x9f, 0x24, 0x45, 0xdf, 0x4f, 0x9b, 0x17,

    0xad, 0x2b, 0x41, 0x7b, 0xe6, 0x6c, 0x37, 0x10

  };

uint8_t Key[16Y] =

  {

    0x2b, 0x7e, 0x15, 0x16, 0x28, 0xae, 0xd2, 0xa6,

    0xab, 0xf7, 0x15, 0x88, 0x09, 0xcf, 0x4f, 0x3c

  };

uint8_t IV[16] =

  {

    0xf0 , 0xf1 , 0xf2 , 0xf3 , 0xf4 , 0xf5 , 0xf6 , 0xf7,

    0xf8 , 0xf9 , 0xfa , 0xfb , 0xfc , 0xfd , 0xfe , 0xff

  };

const uint8_t Expected_Ciphertext[64] =

  {

    0x87, 0x4d, 0x61, 0x91, 0xb6, 0x20, 0xe3, 0x26,

    0x1b, 0xef, 0x68, 0x64, 0x99, 0x0d, 0xb6, 0xce,

    0x98, 0x06, 0xf6, 0x6b, 0x79, 0x70, 0xfd, 0xff,

    0x86, 0x17, 0x18, 0x7b, 0xb9, 0xff, 0xfd, 0xff,

    0x5a, 0xe4, 0xdf, 0x3e, 0xdb, 0xd5, 0xd3, 0x5e,

    0x5b, 0x4f, 0x09, 0x02, 0x0d, 0xb0, 0x3e, 0xab,

    0x1e, 0x03, 0x1d, 0xda, 0x2f, 0xbe, 0x03, 0xd1,

    0x79, 0x21, 0x70, 0xa0, 0xf3, 0x00, 0x9c, 0xee

  };

Once the function �STM32_AES_CTR�_Encrypt is called, I don't get the expected_ciphertext.  I got these data instead:

0x70, 0x2b, 0x25, 0x75, 0x00, 0x00, 0x00 � 

I�m trying to debug on hardware based on STM32F030C8, and also SIMULING by Software . The result is the same.

Does anybody knows why?

Any help would be much appreciated.

Thank you in advance,

Regards.

#crypto-aes-encrypt-stm32
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Amel NASRI
ST Employee
Posted on May 27, 2016 at 16:59

Hi nator.spanking,

The same example is working as expected with my Nucleo F030.

I got a similar result as yours when ''

Crypto_DeInit'' is commented.

Please check that this function is called in your project.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

spankingnator
Associate II
Posted on May 30, 2016 at 13:08

Thanks for your answer Mayla.

Yes, “Crypto_DeInit()� function is called before to STM32_AES_CTR_Encrypt()

As I told, I have not modified anything of the example.

The example that I’m testing is located in the next path of the Crypto Package provided by ST:

…\STM32 Cryptographic library package V2.0.6\Project\STM32F0xx_Cryptographic_Templates\EWARM

I also tried to modify optimizations on IAR Workbench (7.30), but I got the same bad result.

Also tried to change CTR by CBC encryption method and the result again is wrong.

Any help or idea is welcome.  I’m in a hurry.

Thanks

Regards

spankingnator
Associate II
Posted on May 31, 2016 at 14:45

Hi,

Already tested with CTR and CBC encryption methods. None of them return expected data.

:(

Thank you.

Regards.

Posted on June 01, 2016 at 02:14

The crypto library are STM32 locked via the CRC peripheral, if that test fails bogus results are delivered.

I'll take a look at the library some more.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 01, 2016 at 03:31

Well adapted and tested the F0 code on a NUCLEO-F030R8, adding output via USART2, and compiling in Keil.

Output for the test case appeared to work fine.

For good measure I also checked the F4 code on the STM32F407-DISCO

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
kesavan
Associate
Posted on September 01, 2016 at 19:30

I had a similar issue with an F4 and eventually fixed it by enabling the CRC module. In my case, it meant calling

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE);

Posted on April 12, 2018 at 12:23

Thanks for Your Reply, It solved my Problem