User Activity

Hello.To generate a multiplatform code I defined a SW architecture and packaging as follow :Build system :Vendor package can use the cdt project to generate the BSP (cdt builder is the only toolchain supported for system init code generation )Applica...
Posted on June 25, 2018 at 19:53For a customer I want to set RDP Level1 on STM32F4, and put in first sector a bootloader that manager a jump to DFU for device upgrade.I set the RDP L1 by code at init, and disable it with STMCubeProgrammer.Will the I...
Posted on February 05, 2018 at 19:47We're using STMCube to integrate two types of NOR Flash : MICRON and CYPRESS.We are using the HAL_NOR_ProgramBuffer() function, memory data with = 16 bits.Some tests showed that we could not write over the first o...
Kudos from
Kudos given to