STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 CryptoLib - Verifyin on Linux machine

Posted on February 13, 2017 at 13:01Hello everybody,I'm tryin to make a Nucleo-F401 sign a message and then verify this message on a Linux machine. Currently I am able to inject both private and public key into the STM32F401RE (and, starting from EC...

Secure Boot on STM32L475 Discovery IoT kit

Posted on March 17, 2018 at 20:14Hi I want to PORT X-CUBE-SBSFU on to STM32L475 Discovery IoT kit.I want to know what are the initial steps i need to do for PORTING SBSFU on any nucleo Board.Thanks Phanirajkiran#iot-node #device-security #secure-boo...

Secure Boot On STM32L4RQX

Posted on March 12, 2018 at 07:21Hi How do i proceed to write a &sharpsecure boot on STM32L4RXX, with out &sharpHW Crypto. I need to make it by Software later i want to use the HW Crypto provided. Thanks.,Phani#secure-boot

Enable and disable write protection stm32l4

Posted on March 05, 2018 at 19:18I am new to stm32 micro-controller.  I have a question regards to how to enable and disable write protection with stm32l4 chip.  My goal is first I will check if user application is write protected or not, if it is t...

Use stm32 crc to compare DS18B20 crc

Posted on February 25, 2018 at 11:10Hello friend,I have DS18B20. And I read his uniq ID with CRC.And I know, that STM has crc calculator. So I read data from DS18B20: 0xab 0x1 0x4b 0x46 0x7f 0xff 0x5 0x10 : CRC 0x92And I use internal calculator on ...

STM32-CRYP-LIB download problem

Posted on February 14, 2018 at 18:39Hy.I would like to download the crypto library. When I click the request software button, a form shows up. I fill the form correctly, but nothing happens, I cannot download the software.I really need the library. ...

CRC32 calculation in C#

Posted on August 04, 2014 at 10:47 Hi, I created a C# class which calculates the CRC32 checksum exactly like the STM This may be useful to others: using System; using System.Collections.Generic; using System.Linq; using ...

RSA CRYPTO LIBRARY

Posted on February 01, 2018 at 14:46Hi.I'm using an RSA cryptographic library and I have a big issue with the verification process.ST crypto library for RSA has a 'standard' module, message, key pairs and signatures in its main program.I need to use...

Trouble with the CRC unit on STM32F407

Posted on January 17, 2018 at 10:52Hello everyoneI have some trouble with the CRC unit on my STM32F407 MCU.Before each time I am going to use it to calculate a checksum, I reset it and after doing so I double check that the CRC data register (CRC_DR...

Nils B by Associate II
  • 5689 Views
  • 11 replies
  • 0 kudos