2019-10-15 1:55 PM
If the Read Protection is set to RDP Level 1 in the Option Bytes, does the above claimed vulnerabilities affect STM32F7xx or STM32H7xx MCUs?
2019-10-15 5:20 PM
> If the Read Protection is set to RDP Level 1 in the Option Bytes, does the above claimed vulnerabilities affect STM32F7xx or STM32H7xx MCUs?
That's a question you should ask the authors of the given paper:
Marc Schink
Fraunhofer Institute AISEC
marc.schink@aisec.fraunhofer.de
Johannes Obermaier
Fraunhofer Institute AISEC
johannes.obermaier@aisec.fraunhofer.de
The paper does not mention either level of RDP. They deal with PCROP, which is something different.
They don't even acknowledge existence of RDP, which is sort of unfair, but then it would decrease the sensational value of their paper.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.