STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SECoreBin postbuild.sh

Hello guys,I was setting up my STM32CubeIDE to use the SBSFU sample projets. I'm facing a issue with SECore engine, more specific the postbuild.sh script.When i compile SE, i get the following message:ln: failed to create symbolic link '../../postbui...

MBuen.1 by Senior
  • 1618 Views
  • 2 replies
  • 0 kudos

SBSFU with STM32F469/STM32F479 and SPI flash

Hi everyone,I am using STM32F469/STM32F479 and want to integrate SBSFU with an SPI flash. Basically the active image is in MCU's 1 Mbytes flash and downloaded image is in the external flash. There are several questions I would like to know before I s...

SL61 by Associate II
  • 1165 Views
  • 1 replies
  • 0 kudos

Ethernet Init fail with sbsfu bootloader

Hello everyone!I am testing my own firmware with the sbsfu bootloader (stm32h723). I have the problem that when the MCU is trying to set up the ethernet the board will die.The ETH region is protected by MPU and before enabling it in my app I disable...

Resolved! SBSFU SECoreBin debug

Hi,I am trying to use external flash to download the FW and facing issue at FWPartialTag comparison. I want to debug SECoreBin project to see what is going on while I am in debugging SBSFU project.Is this debug jump possible? If so, Could you please ...

ANaga.2 by Associate II
  • 2209 Views
  • 3 replies
  • 0 kudos

After downloading a new firmware blob via YMODEM transmssion, why does SBSFU report that installation is not validated instead of installing the new firmware?

We implemented an OTA update procedure where we provide an STM32L476 with a new firmware via serial using the Ymodem protocol in a two-image SBSFU configuration.We are executing long-running tests in which we use the same firmware image to test the u...

tomptz by Associate II
  • 1857 Views
  • 2 replies
  • 0 kudos