Skip to main content
Pavel A.
September 20, 2020
Solved

Where is hardware accelerated crypto lib for STM32H753?

  • September 20, 2020
  • 8 replies
  • 3108 views

I have a recent download of en.x-cube-cryptolib_3.1.0.zip and en.patchx_cryptolib_3-1-3.zip.

The former contains AccHw_Crypto subdirectory with subdirectories for F2, F4, F7 and so on but no H7.

Subdirectory for H7 exists only under Fw_Crypto.

In en.patchx_cryptolib_3-1-3.zip there are subdirectories for G0, G4, L5, WB and H7A3. All these, I guess, are software only?

Which package contains hardware accelerated library (AccHw_Crypto) for H753 ?

Thanks,

-- pa

This topic has been closed for replies.
Best answer by Jocelyn RICARD

Hello Pavel,

I'm sorry, I'm not dedicated to community support. Try to answer the best I can. Also, for some reason I don't receive all notifications...

Clive gave the right answer. STM32H753 has no acceleration IP for asymmetric crypto (Acceleration IP called PKA is available on other families such as STM32WB and STM32L5)

So, if you need to perform PKCS#1v1.5 on H7 you have to use the software implementation.

Also, as Clive mentioned, the hash part (which result is usually used as input of the signature check) can be accelerated.

Symmetric authentication is obviously less robust as you need the private key to check the signature.

You have exemples of this here: STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Examples\HASH\

To understand the differences I would suggest having a look to the MOOC basic of cryptography which is part2 of the following MOOC series

https://www.st.com/content/st_com/en/support/learning/stm32-education/stm32-embedded-security-learning-journey.html

Best regards

Jocelyn

8 replies

Tesla DeLorean
Guru
September 20, 2020

Can't you just use the HAL?

STM32Cube_FW_H7_V1.7.0\Projects\STM32H743I-EVAL\Examples\CRYP

STM32Cube_FW_H7_V1.7.0\Projects\STM32H7B3I-EVAL\Examples\CRYP

STM32Cube_FW_H7_V1.7.0\Projects\STM32H7B3I-EVAL\Examples\OTFDEC\OTFDEC_ExecutingAesInstruction

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
Pavel A.Author
September 28, 2020

I need RSA PKCS1v15 (verify RSA signatures). The HAL examples for CRYP and HASH don't seem to support this directly.

Hence I need the crypto library...

-- pa

Tesla DeLorean
Guru
September 29, 2020

Does the HW support that? I'd presume the SHA256 or whatever hash you're signing, but not the signing itself?

Not sure who the ST Crypto guys are here, if this is a commercial project press your FAE

@Imen DAHMEN​ @Amel NASRI​  can you assign this to those responsible for the H7 CRYPTO, thanks.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Technical Moderator
September 30, 2020

Hello @Pavel A.​ ,

Based on UM1924 - Table 4. STM32 crypto hardware acceleration libraries, the HW accelerated library for STM32H7 is not supported.

I propose FW library, as there is little difference between Lib FW and HW regarding performance and code size.

Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks