STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SBSFU - ECCKEY and AES Key

Hi,I have a bit trouble understanding the two keys in the SBSFU and which pairs is actually used. From AN5056, chapter 5 there is stated how to generate the two different methods and the AES key I could successfully adjust. With the ECCKEY method and...

0693W00000JMeQYQA1.png
STsch.1 by Associate III
  • 1688 Views
  • 1 replies
  • 0 kudos

Resolved! Can I use Trustzone with DBANK=0 ?

The examples in CubeU5 package always states to activate dual bank mode, when using TrustZone. Can't you use single bank mode and just allocate specific sectors to be secure?Is it possible to use TrustZone without dual bank? Some types don't have it....

LBöhm.1 by Associate III
  • 1326 Views
  • 1 replies
  • 0 kudos

X-CUBE-CRYPTOLIB, is it necessary to request the software?

Hi,I'm working on a project that needs AES256 encryption, I requested the X-CUBE-CRYPTOLIB software, but it's being validated by STM32, my question is, why does this validation exist? Is there any criteria for them to make the software available? Wha...

VPatr.2 by Associate II
  • 1250 Views
  • 1 replies
  • 0 kudos

Resolved! Cannot debug the AWS demo on B-L475E-IOT01A1

Dear all,For an IoT project I would like to run the demo of the AWS package provided by ST but for some reason I could not manage to debug the demo project.To do so I have downloaded the X-CUBE-AWS_v2.0.0 package and used the following ressources : S...

VSpad.1 by Associate II
  • 3822 Views
  • 7 replies
  • 0 kudos