User Activity

Hi,What am I missing ?The connection to the event source is grayed and non selectable, see screen copies of the configuration below.  
The ECDSA implementation in cryptolib does not provide means of implementing ECDSA without a random number. RFC6979 is a secure way of doing ECDSA without a random number, it is used in the blockchain implementations (bitcoin, ethereum)
Hi all,ADC triggering appears to be at half the frequency of the timer, (ie occurs every 2 update events), is this expected ?This is with a STM32F334 progammed using HAL and with code generated by CubeMX.I am reading 14 ADC channels using DMA (2x7 in...
Posted on August 25, 2017 at 20:14Hi all,The signature algorithms (DSA or ECDSA) all require a random number. If this random number can be guessed, the signature becomes weak and the private key can be recovered (cf. the Sony PS3 signature affair).I...
Posted on February 27, 2016 at 01:27-removed- case solved #stm32f746-cubemx-timer-tim5