STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I'm not able to make working the NUCLEO-L432KC example

I wont to test the L432KC example on a NUCLEO-L432KC board"\SBSFU\STM32CubeExpansion_SBSFU_V2.6.0\Projects\NUCLEO-L432KC\Applications\1_Image"I have created correctly a new workspace and imported the necessary projects. All compiles fine and I get "S...

GMG by Associate III
  • 1552 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0 CRC16 mismatch.

Hi,I am trying to run the CRC calculation with the STM32G031 but the results do not match. The result of the CRC16_CCITT_FALSE should be 0x29B1 according to http://www.sunshine2k.de/coding/javascript/crc/crc_js.html but I get 0x277F.You can find my i...

FRieb.1 by Associate III
  • 3792 Views
  • 7 replies
  • 0 kudos

Resolved! Serial DFU of Secure Firmware Fails

I'm attempting to use the serial bootloader to load a secure firmware image to an STM32L5 using STM32CubeProgrammer. I can successfully connect to the board in bootloader mode and perform a full-chip erase, but attempting to download the image (eithe...

MBand.3 by Associate III
  • 1325 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H753 with "secure area": how to un-brick?

So I have a STM32H753 with active "secure area" - but the code in the secure area is buggy and hangs before jumping outside.Is there a way to erase the MCU and recover, or it is bricked?No RDP is set.

Pavel A. by Super User
  • 1125 Views
  • 1 replies
  • 0 kudos

CRC Calculation for 8-bit values

I am experimenting with CRC Calculation on a STM32F4-Discovery.As I have seen in the reference manual this MCU is using CRC-32 used in Ethernet. I am also using https://crccalc.com/ (CRC-32/MPEG-2) to validate the results.I just activate the CRC in C...

Application hangs when doing a remote update

The details of this project are like this. I have a working product on the F417 that I wish to add Remote update capabilities to.Product is already deployed with SBSFU and updates using Ymodem through the UART work fine.What I am trying to add on now...

Eugene G by Associate III
  • 2145 Views
  • 2 replies
  • 0 kudos

SBSFU - ECCKEY and AES Key

Hi,I have a bit trouble understanding the two keys in the SBSFU and which pairs is actually used. From AN5056, chapter 5 there is stated how to generate the two different methods and the AES key I could successfully adjust. With the ECCKEY method and...

0693W00000JMeQYQA1.png
STsch.1 by Associate III
  • 1681 Views
  • 1 replies
  • 0 kudos