STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SFI : Error: RSS internal system error or License is invalid!

Device details :ST-LINK SN : 002F003F3137510539383538ST-LINK FW : V3J9M3B5S1Board    : STLINK-V3SETVoltage   : 3.76VSWD freq  : 24000 KHzConnect mode: Hot PlugReset mode : Software resetDevice ID  : 0x480Revision ID : --Device name : STM32H7A/BFlash ...

0693W00000NrUfRQAV.png
Grogu by Associate III
  • 3806 Views
  • 5 replies
  • 0 kudos

Resolved! Is the STM32H753 a drop-in replacement for STM32H743?

I know that STM32H753 is pin-compatible to STM32H743, and as far as I know also code-compatible for most intents and purposes. The only difference seems to be the Crypto hardware acceleration. So I assume that I can run code from H743 on the H753 wit...

JArwe.1 by Associate II
  • 2601 Views
  • 2 replies
  • 0 kudos

Using Tamper with TF-M in STM32U5

Hi,In TFM and SBSFU applications, by default the anti-tamper protection is enabled for both internal tamper events and external tamper events. It is activated at the start of TFM_SBSFU_Boot, and remains active.In case of tamper detection, sensitive d...

ZKRAC.1 by Associate II
  • 1834 Views
  • 1 replies
  • 0 kudos

cmox_rsa_pkcs1v15_verify() returns CMOX_RSA_AUTH_FAIL

Working on a project using STM32G071CBT6. Using STM32CubeExpansion_Crypto_V4.0.1 Projects NUCLEO-G071RB Applications RSA PKCS1v1.5_SignVerify RoutinesTrying to sign a 138 byte msg.cmox_rsa_pkcs1v15_verify() returns CMOX_RSA_AUTH_FAILAny suggestions?

YGarg by Associate II
  • 1792 Views
  • 2 replies
  • 0 kudos

SBSFU keeps rebooting - SE_IsUnprivileged() always return 1

Hi,I'm trying to implement secure boot and secure firmware update on STM32F415RGT6 but I'm having hard time with SBSFU code.I already compiled the example STM32F413H-Discovery making adjustment for flash and ram in linker file. Then I runned the SBSF...

0693W00000Nt1U6QAJ.png 0693W00000Nt1UYQAZ.png
G.Poma2 by Associate
  • 1138 Views
  • 1 replies
  • 0 kudos

I have a product going to market that uses a stm32l486xx processor. There are two CVEs that apply to this micro, CVE-2021-29414 and CVE-2020-27212. Can anyone tell me what the first CVE means?

Also, apparently CVE-2020-27212 means that you can bypass flash readout protection. Is that a correct reading of that CVE? Note that searching both the ST main site and the community site produce no hits for either CVE, and trying to determine the ...

Resolved! Can SBSFU internal loader enabled in RDP_LVL 2 mode ??

We have plan to support application down-loader from Application context. It means Application has ability to receive new application over the air. Not SBSFU.In case of Active application got corrupted somehow, then SBSFU is locked the MCU, as we los...

SPati.7 by Associate III
  • 4687 Views
  • 13 replies
  • 0 kudos