STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Could TCPP01-M12 be used without the N-MOSFET?

We have a wide-input power management ic with buck-boost converter. 28V VBUS is not a problem. So is it possible to eliminate the N-MOSFET (at least in Sink mode)? If it is OK, what is your recommendation for connections of IN_GD, Gate, and Source pi...

matianfu by Associate II
  • 225 Views
  • 1 replies
  • 1 kudos

STM32F0 USB Audio Record

Is there any working example to do USB Audio Recording using the STM32F0? I need to send audio received by the I2S port on the STM32F0 and send it out to the host PC via USB. I have seen AN4711 and also have the Record working on the F7 with the hel...

EThur.1 by Associate
  • 304 Views
  • 0 replies
  • 0 kudos