STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407G Dev-Kit LD1 Noise

Hi! I've been following this tutorial to enter the world of audio dsp. The issue is that when I connect the board via USB, LD1 is always on (red) and I can hear a bunch of white noise at my output. When I power the board externally via 3V, LD1 starts...

Resolved! X CUBE USB AUDIO not recognized as audio device

Hello, I want to use X CUBE USB AUDIO examples in X CUBE IDE.After generating the binary code (without errors) and flashing the binary code via DFU, the card is not recognized as an audio device, I tried on all 4 projects. I unplugged USB, do reset, ...

Loulou by Associate II
  • 1356 Views
  • 10 replies
  • 0 kudos

USB Type-C IC suggestion

Hi,I'm looking for some suggestions for the implementation of a self-powered and DRD (Dual Role Data) system provided with USB Type-C connector, but without PD support.I found two different solutions:1) Using a configuration channels protection IC (T...

i2s driver audio chip

Hello, I am a student. I want to use I2S through STM32L051K8U6N to complete the acquisition of the MP34DT04 sensor, but I have not found any information about libPDMFilter_CM4F_Keil.lib, keil library and IAR library similar to this. If it is convenie...

Daqiang by Associate II
  • 253 Views
  • 0 replies
  • 0 kudos

Safety Test Library : rom test fail issue

I'm using the STM32F767 MCU and Keil compiler. The Keil version is Fusa 16.2. When applying the STL library in the Keil compiler environment, a rom test failure occurs.STL version is 4.0, and it was applied as in the guide document, but STL_Lib respo...

제목 없음.png
MLee.14 by Associate
  • 201 Views
  • 0 replies
  • 0 kudos

VDD pin connection of STUSB1600

Hi, I am trying to use STUSB1600 as a front end interface to my USB Type-C connector and interface it with STM32L4R9 series microcontroller. It is a dual role type application but with no power delivery. Unable to understand why VDD of STUSB1600 is c...

MoniR_1-1711709267257.png MoniR_2-1711709502506.png
MoniR by Associate
  • 419 Views
  • 4 replies
  • 2 kudos

SPDIF IN/OUT check (IEC61937)

If there is an EVM that meets all or part of the following conditions, I would appreciate your recommendation. * I am looking for a possible EVM because I want to check whether a file that should not be played with SPDIF in due to license restriction...

pasach by Associate
  • 423 Views
  • 0 replies
  • 0 kudos