How to connect speaker in STM32U5 [B-U585I-IOT02A ]
Hello Community,I want play audio from stm32u5, to any speaker. Is there any method to play audio from stm32u5 or way to connect speaker to stm32u5.
Hello Community,I want play audio from stm32u5, to any speaker. Is there any method to play audio from stm32u5 or way to connect speaker to stm32u5.
Hi.I used USB_OTG_FS as Audio Device Class on STM32F407-discovery.I connected PC and STM32F407-discovery with USB device.When I played music, sometimes sound is not occurred on STM32F407-discovery.I found that epnum in USBD_LL_DataOutStage is always ...
Hello,I am developing a functional safety project in IEC 61508 standard, which requires static and unit testing of all of the functions in the project. My question is, "Can I use auto-generated CubeMX configuration functions or the HAL library in my ...
Tried a lot of stuff, including STM32CubeExpansion_MEMSMIC1_V5.7.0, STM32CubeExpansion_USBAudioStreaming_V1.0.0, STM32CubeFunctionPack_SMARTMIC1_V2.3.0, porting existing apps to STM32G4 with no success.The USB device gets appeared in Windows OS in ~5...
Greetings to the ST community,I was using the example project provided by ST in "STM32F769I-Discovery\Applications\Audio\Audio_playback_and_record\EWARM" and found out that voice was being output through the headphones. However I connected speakers t...
I am using STMCubeIDE latest and an F411CE.I used the MX wizard to enable USB_Audio class device set to 48000 s/sI configured an I2S with master clock on IS2.It plays whether I start the circular DMA in the AUDIO_Init function or in the AUDIO_CMD_STA...
I'm trying to make 2 DRP 100w ports but I can't find many related resources. Can anyone help by providing a sample code or related resources.
Hello, I am developing a home appliance application on an MCU STM32G070CB using X-CUBE-CLASSB package and IAR EWARM IDE V8.32.4. I used NUCLEO-G070RB for the early development. The app ran fine until I turned on the SRAM parity check in the options b...