Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VBUS monitoring not working on STUSB1602

Hi guys ! I am trying to implement a USB-C powering and communication between 2 of my devices. There is no Power Negociation implemented yet. The default voltage is 5V.I want to make sure my source device is safe so I would like it to shut down VBUS ...

0693W00000QOOZCQA5.png
VSpad.1 by Associate II
  • 1433 Views
  • 1 replies
  • 0 kudos

STUSB4500

Can the STUSB4500 support a USB C DRP and USB PD (sink-only) application using the SOM OTG interface illustrated above? Can it drive the VBUS, OC, and ID inputs and receive the EN output? We would like our product to serve as USB UFP (device), USB DF...

EHD by Associate II
  • 1223 Views
  • 1 replies
  • 0 kudos

LE coded PHY devices compatibility?

Anyone aware if iPhones/ Androids accepting LE coded PHY?If so, starting at which versions do they start working? I saw some info dating from 2020 or early 2021 so I'm wondering if someone has a more recent answer.

CHoul.1 by Associate
  • 794 Views
  • 0 replies
  • 0 kudos

product request: STULPI01 LQFP package?

hi various SOCs in STM32 family e.g. stm32f407ve, and many in the F7, H7 series features a "USB 2.0 high-speed/full-speed device/host/OTG controller with dedicated DMA, on-chip full-speed PHY and ULPI"But your STULPI01 is a μTFBGA36 package. https://...

andrewg by Associate III
  • 1002 Views
  • 0 replies
  • 0 kudos