I want to connect 7 LED's on one output in series, using a current of 20 mA. Each LED can have a forward voltage of 3V, which means 7 x 3 = 21 V. I want to use a power supply of 24V.I read in the specifications that the max Vo (Output Voltage) is rat...