Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem Using X-CUBE-BLE1

Hello, I'm developing a project on a NUCLEO WL55JC1 board. I require Bluetooth communication between my board and some sensors, so I'm implementing the BLUENRG-M0A module and the X-CUBE-BLE1 pack. Similarly, I'm using the SampleApp example as a base....

Resolved! SIM7022 esim

Can you tell me is the SIM7022 is also compatible with the ST4SIM-200M. Best regards Peter Jonkers

Foggy by Associate
  • 3048 Views
  • 3 replies
  • 0 kudos

Dual STUSB4710 Power Management

I am designing a usb type-c charger. I want to use 2 microcontroller and 2 STUSB4710.Type-C Output will be 20V 3.35A 67W.I want to do power management between these USB Type-C outputs.I have questions. Can you please answer them? 1. Are there any I2C...

Resolved! Camera controller

Hey team,I wanted to check if there is any bridge IC  that can convert parallel camera interface data to USB 3?And/orDo we have anything that can convert MIPI CSI-2 to USB 3? - again for a camera IC.Thank you for your help!

Ilker123 by Associate
  • 1783 Views
  • 1 replies
  • 0 kudos

Resolved! Zigbee identify and groups cluster

Hi evryone,I've been trying to work on Zigbee communication for a while now, so far I've just learned how to read and write attributes. Now I'd like to try to learn how to use cluster Identify and groups, but I dont understand several thing, so I nee...

CH3 by Associate II
  • 17001 Views
  • 12 replies
  • 1 kudos

Resolved! BlueNRG-LP I2C1 and I2C2 coexistence

hello community,I´m using PB10/PB11 as I2C1 and PB6/PB7 as I2C2.I2C1 works correctly.But I2C2 not, after reset on PB6 and PB7 I just get some messy signals as below, It seems the I2C2 is not initialized with succcess.Actually the both I2C are initial...

Danny0007_0-1706436538253.png Danny0007_1-1706436961888.png