cancel
Showing results for 
Search instead for 
Did you mean: 

TS555 Reset levels

TomLH
Associate

Hi. From DS of TS555 I'm not clear about RESET acitve low level. In DS VRESET is given 0.4V(min), 1.1V(typ), 1.5V(max) for +25°C and 0.3V...2.0V for whole temp range, see attachement
Can someone help to get min/typ/max level for RESET is active and the level RESET is inactive at +5V supply and -25°C....+85°C.

Thx Tom

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @TomLH, to the community!

Well, the TS555 was developed decades ago and the specifications found in the data sheet were set at that time. The 0.4…1.5V only applies to 25°C, at other temperatures it must be ensured that RESET can be triggered correctly, i.e. the voltage must drop to a level of ≤0.3V to trigger. 

On the other hand, it must also be taken into account that RESET may only be triggered from 2.0V.

Typically, a temperature other than 25°C will be present, so the full temperature range specification applies so that STMicroelectronics can guarantee the parameters under all circumstances.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @TomLH, to the community!

Well, the TS555 was developed decades ago and the specifications found in the data sheet were set at that time. The 0.4…1.5V only applies to 25°C, at other temperatures it must be ensured that RESET can be triggered correctly, i.e. the voltage must drop to a level of ≤0.3V to trigger. 

On the other hand, it must also be taken into account that RESET may only be triggered from 2.0V.

Typically, a temperature other than 25°C will be present, so the full temperature range specification applies so that STMicroelectronics can guarantee the parameters under all circumstances.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.