Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-2, Whitelist and Advertising

Hej Folks,I have an application with multiple BlueNRG-2s. There are 1 Master and up to 5 Slaves. I would like to connect the master to these 5 Slaves only, so no other device can connect to them and vice versa. I thought about using a whitelist. Curr...

Yoschii by Associate
  • 1117 Views
  • 0 replies
  • 0 kudos

STEVAL-IDB012V1 / ARDUINO

Hello, please how can I connect a STEVAL-IDB012V1 board with an arduino (if it is possible of course), if not is there a mobile application with which I can connect to this board and retrieve the pressure and acceleration values?

ljm by Associate III
  • 1335 Views
  • 3 replies
  • 0 kudos

IDB011V2 BlueNRGLP device name

Hi community,in the example code BLE_SensorDemo_BlueMSapp there are two places where the device name is set, this one looks reasonable for the device name, but I tried to change it, actually this does not affect the device name, which is shown in the...

Danny0007_0-1711274127240.png Danny0007_1-1711274180208.png

STM32f407VET6 : Dry contact and Wet contact

Dear Team,we are going to develop an IO module series with digital Inputs/Outputs. We have developed previous all products using STM32F407VET6,100pins controller and for IO modules series we will be using ST controller only but rest components are ye...

ATPL by Associate II
  • 981 Views
  • 0 replies
  • 0 kudos