Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I use of SPIRIT1 for MICS band(403MHz)?

Posted on January 15, 2015 at 03:30Hi all,I have a project in which I have to use MICS band for data telemetry in an implantable device. Can I use the SPIRIT1 for MICS band which centers at 403MHz? (I think the TI CC1101 can be configured to do it, ...

quyen by Associate
  • 1047 Views
  • 1 replies
  • 0 kudos

Spirit1 Evaluation

Posted on December 19, 2014 at 21:13From the landing page on the SPIRIT1 Radio, if i want to operate 915/922 MHz Band - what is required to get started?  Can I use two of the Dongles evaluation modules - STEVAL0IKRV001V5 (on a computer perhaps with ...

rick2399 by Associate II
  • 1127 Views
  • 1 replies
  • 0 kudos

Spirit1 DK error

Posted on September 29, 2014 at 11:06Hi, I just installed the STSW-CONNECT009 pack, and upon starting the Spirit1 DK I get an error. The error in the error-log.txt is the following: ''local variable 'key' referenced before assignment''Could anyone h...

molnarda by Associate II
  • 3834 Views
  • 9 replies
  • 0 kudos

STEVAL-IDW001V1 Troubleshoot

Posted on November 21, 2014 at 03:44Hi, I am working with evaluation board (STEVAL-IDW001V1) equipped with the WiFi module (SPWF01SA.11), and having trouble with updating the firmware (FW) to the board.  I followed the instructions to have BOOT0 hig...

mvvu by Associate II
  • 4381 Views
  • 14 replies
  • 0 kudos

SPWF01S Station connection problems

Posted on December 17, 2014 at 10:35Hi all, I'm using the WiFi module to connect to infra WiFi in socket server mode. The module return (through serial link) that connection to WiFi is OK. But sometimes, in the WiFi router interface (a Freebox), the...

cbertrand by Associate II
  • 6267 Views
  • 16 replies
  • 0 kudos

firstset.cgi psk not crunched

Posted on December 18, 2014 at 10:13We are currently developing a product that uses the SPWF01S module running firmware:140623-cd34ea1-SPWF01S.Our product relies on the firstset.cgi to connect to a network, the situation is as follows: A microcont...

jimmicola by Associate II
  • 2487 Views
  • 6 replies
  • 0 kudos

Where is X-CUBE-IDB04_L0 software?

Posted on December 04, 2014 at 11:02Apparently there should be ''X-CUBE-IDB04_L0 STM32Cube expansion software for X-NUCLEO-IDB04A1'' available here, but it is not present on that web page: http://www.st.com/web/en/catalog/tools/PF261371 and describe...

charles23 by Associate III
  • 895 Views
  • 1 replies
  • 0 kudos

BLE IDB04A1 and Nucleo STM32F302R8

Posted on October 23, 2014 at 14:24Hi all, I'm new in this forum and apologize if my question already exists (but I haven't found)... In these days, I spent a lot of my  time trying to use Bluetooth IDB04A1 with a Nucleo STM32F302 board without resu...

marcello by Associate
  • 1287 Views
  • 3 replies
  • 0 kudos

BlueNRG Set Advertising Data

Posted on December 10, 2014 at 07:41Hi, I'm trying to set the advertising data and make it advertise, but the client doesn't detect any of the data. Here are the command that I use: HCI_LE_Set_Advertizing_Parameters HCI_LE_Set_Random_Address HCI_...

dimitar by Associate II
  • 1029 Views
  • 1 replies
  • 0 kudos