Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Data Mode to Command Mode

Posted on January 22, 2016 at 10:02Hi!I have connected my Wi-Fi module  with a client and now I am getting the commands+WIND:61: Incoming Socket Client :172.31.142.2+WIND:60: Now in Data Modenow I want to get back to  command mode.I have tried hitti...

Nandy K by Associate II
  • 3067 Views
  • 13 replies
  • 0 kudos

How to customize the advertising packet?

Posted on January 09, 2015 at 18:46Hi, I'm trying to customize the advertising packet, but it's unsuccessful so far. I use STEVAL-IDB002V1 BlueNRG HW v3.0BlueNRG FW v6.4Motherboard FW v1.4Since the command ACI_GAP_SET_DISCOVARABLE doesn't give much ...

dimitar by Associate II
  • 5503 Views
  • 11 replies
  • 0 kudos

ip_sockd_timeout usage

Posted on January 20, 2016 at 16:08Hello all,I'm using a SPWF01SA.11 as a web server. It is coupled with an host MCU that process the http protocol: the internal web server on the module is disabled (ip_use_httpd = 0), and I have opened the socket s...

Test-report request

Posted on January 20, 2016 at 08:54Hello all,we need the test report about the ETSI EN 300 328 certification in order to proceed with the certification of our final product. Thank you,Marco

X-CUBE-BLE1 expansion software

Posted on December 04, 2015 at 10:11Hi, I have the STM32F411 Nucleo with  X-NUCLEO-IDB04A1 BLE expansion module.I attempted to download the X-CUBE-BLE1 expansion software from the link below, but no ''download'' button available. http://www.st.com/...

Use of BlueNRG_Stack_IFR_Updater

Posted on January 13, 2016 at 13:34Hi ,        BlueNRG_Stack_IFR_Updater    What is the use of above application which is available in the    ''  \BlueNRG DK 1.8.0\Projects\Projects_Cube '' -- Regards Ratheesh T

updated UM1755 doc?

Posted on February 03, 2015 at 08:49Hi everyone, I was wondering if there is an updated version for the UM1755 which (partially) describes the commands available for the BlueNRG chipset. I can't find decoding scheme for the VS HCI events for example...

philippe1 by Associate II
  • 3595 Views
  • 11 replies
  • 0 kudos

BlueNRG Set_Scan_Parameters not recognized

Posted on January 10, 2016 at 18:37Hi,I'm interface the BlueNRG directly (not using the ACI stack), and having problems programming a Central device when trying to configure scan parameters. Here it is my sequence of events and commands:1) 04 FF 03 ...

raymel by Associate
  • 1235 Views
  • 3 replies
  • 0 kudos