2015-03-25 8:15 AM
Hello,
Can you clarify how work function hci_le_transmitter_test?I could not
find any
description
of this method.
I found that the test run for just a second, but I thought that the test will continue until the command hci_le_test, is not it? Regards, Andrei Kukenov.2015-03-27 5:44 PM
Interesting question - so I looked at section 7.8.29 of the BLE spec to see this:
HCI_LE_Transmitter_Test 0x001E TX_Channel, Length_Of_Test_Data, Packet_Payload Status Trying to study the Le Rx and Tx test commands, I am going to guess that this Le Tx test command parameter: Length_Of_Test_Data Really means, ''total number of test data packets to transmit'', and then that number specified should match the Le Rx test done result on the other side of the link, unless the Le Tx test returns an error code (i.e. I could only send 17 of 23 test-pattern packets).2015-04-03 3:21 AM
Hi,
for futher details, please se the AN4494 (section 7 Packet exchange test) Regards, GM