cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01SC.11 send data to Server by TCP Socket.

Khoa Tran
Associate II
Posted on March 27, 2015 at 09:51

I use SPWF01SC.11to send data to server (about 6KB every 4 minutes).I split data to 2 packages (3KB each package) then send to server by TCP Socket.But sometime 1 package is lost.

Can anyone help me to solve this problem?My mail is 

mailto:khoatran@digisensor-co-ltd.com

 </span>

Thank you.

Tran Khoa.
This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
Khoa Tran
Associate II
Posted on March 27, 2015 at 10:08

Gerardo GALLUCCI
ST Employee
Posted on March 27, 2015 at 15:42

Hi,

which version are you evaluating?

Can I have a full dump of configuration and status variables?

Thanks, and sorry for the issue!

ciao

jerry

Khoa Tran
Associate II
Posted on March 28, 2015 at 02:10

I use firmware 141106 rel 3.3

# Dumping All Configuration Keys:

#  nv_manuf = ST

#  nv_model = SPWF01SC1

#  nv_serial = 1114E11454

#  nv_wifi_macaddr = 00:80:E1:FF:CD:56

#  blink_led = 0

#  wind_off_low = 0x00000000

#  wind_off_medium = 0x00000000

#  wind_off_high = 0x00000000

#  user_desc = anonymous

#  escape_seq = at+s.

#  localecho1 = 0

#  console1_speed = 230400

#  console1_hwfc = 0

#  console1_enabled = 1

#  sleep_enabled = 0

#  standby_enabled = 0

#  standby_time = 10

#  wifi_tx_msdu_lifetime = 0

#  wifi_rx_msdu_lifetime = 0

#  wifi_operational_mode = 0x00000011

#  wifi_beacon_wakeup = 1

#  wifi_beacon_interval = 100

#  wifi_listen_interval = 0

#  wifi_rts_threshold = 3000

#  wifi_ssid = 44:47:53:32:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_ssid_len = 4

#  wifi_channelnum = 6

#  wifi_opr_rate_mask = 0x00003FCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_mode = 1

#  wifi_auth_type = 0

#  wifi_atim_window = 0

#  wifi_powersave = 0

#  wifi_tx_power = 18

#  wifi_rssi_thresh = 0

#  wifi_rssi_hyst = 0

#  wifi_ap_idle_timeout = 120

#  wifi_beacon_loss_thresh = 10

#  wifi_priv_mode = 2

#  wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_key_lens = 00:00:00:00

#  wifi_wep_default_key = 0

#  wifi_wpa_psk_raw = 84:14:B0:82:F3:D3:2E:24:06:9B:CA:BD:16:B9:9D:D0:40:10:F5:C3:AC:D7:3F:57:C2:39:D3:7D:84:D1:C9:38

#  wifi_wpa_psk_text = 445b926b99

#  ip_use_dhcp = 1

#  ip_use_httpd = 1

#  ip_mtu = 1500

#  ip_hostname = iwm-FF-CD-56

#  ip_apdomainname = captiveportal.net

#  ip_ipaddr = 192.168.0.50

#  ip_netmask = 255.255.255.0

#  ip_gw = 192.168.0.1

#  ip_dns = 192.168.0.1

#  ip_http_get_recv_timeout = 3000

#  ip_dhcp_timeout = 20

#  ip_sockd_timeout = 250

Gerardo GALLUCCI
ST Employee
Posted on March 30, 2015 at 18:48

Thanks for the dump.

I tried to reproduce the issue, but I had no luck. I'll keep on trying...

I'll suggest you to upgrade to near coming FW3.4, when available. There are important fixes, and improved overall reliability. Stay tuned with your local ST support for FW delivery.
Khoa Tran
Associate II
Posted on March 31, 2015 at 03:27

Thank you,

When It is released? I waited for so long.

Sory for my bad English.

Tran Khoa.

Gerardo GALLUCCI
ST Employee
Posted on April 01, 2015 at 12:06

Release planned in 10 working days (after Easter period)

Khoa Tran
Associate II
Posted on April 02, 2015 at 10:52

I send a buffer ex data[5]={0x01,0x02,0x03,0x00,0x04}

I use command

at+s.sockw=00,5

and send data[5] but module wifi only received 3 byte 0x01 0x02 0x03.It pass from byte 0x00.

Is it a bug? 

Gerardo GALLUCCI
ST Employee
Posted on April 03, 2015 at 12:25

Hi,

I try to figure out your use case:

- Your external host sends over UART the AT-command SOCKW(5 bytes)

- Module takes only 3 bytes, and never gives ''OK'' message back to external host

Is it correct?

If you are not using an external host, be sure you are not sending CR and/or LF.

No bug. Let me understand your use case.

Regards

jerry

Khoa Tran
Associate II
Posted on April 06, 2015 at 02:49

I use external host (STM32F401VCT6).

It's correct.Module never gives ''OK'' back,It's wait for 2 bytes.It's like this

char data[5]=

{0x01,0x02,0x03,0x00,0x04}

;

printf(''at+s.sockw=00,5\r'');

printf(data);  //Module never gives ''OK'' It's wait for 2 bytes more.

printf(0x02);

printf(0x03); //Module gives ''OK'' here and TCP Sever receives 0x01,0x02,0x03,0x02,0x03