Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

spirit1 autoack problem

Posted on October 06, 2016 at 11:35We are testing p2p connectivity software on NUCLEO L152RE + X-NUCLEO-IDS01A4. We need to use auto acknowledgement and auto retransmission feature on spirit1. Whatever the application in the SUBG1 package, is not us...

vamsi by Associate II
  • 673 Views
  • 0 replies
  • 0 kudos

Spirit1 / SPSGRF receive

Posted on October 04, 2016 at 16:58Hi,I use the SPSGRF module in 868MHz Narrowband. I search to send packet with this configurations : - Fc = 869.2375MHz- Fdev = 2.7 kHz- Datarate = 4.8 kBit/s- Number of channels : 0- Spacing channel : don't care ? ...

Wireless M-Bus stack

Posted on September 29, 2016 at 13:06Dear Support Team,I want to collect data from 64  heat meters, heat meters are from Danfoss, in mode T1.The purpose of the project is only data collecting from heat meters without decryption, collected data forwa...

klevente by Associate II
  • 673 Views
  • 0 replies
  • 0 kudos

spwf01 module Timing Issue

Posted on September 01, 2016 at 12:45Hi,I observed followings while communicating between two spwf01modules: At the Client side when its try to connect to server I’m using AT+S.SOCKON command to connect. In this command I can pass “ind�? parame...

BlueNRG return/error codes?

Posted on August 29, 2016 at 15:09Hi. I`m implementing BlueNRG based Eddystone beacon. And i have to check GATT Return/Error codes of GATT read/write commands in Android/iOS application. I have no idea about this codes and i found no BueNRG API fun...

Output.cgi and httpdfsupdate

Posted on September 13, 2016 at 14:00Hi I have an issue similar to one raised earlier in the forum but there didnt appear to be a resolution.When I create my own web pages and use the output.cgi as per examples I have found, when I submit the data f...

AP and miniAP difference

Posted on September 12, 2016 at 11:14Hi,I have doubt, what is the difference between AP(Access point) and miniAP.Is there any functionality difference?Is there any less functionality in miniAP compare to AP?Thanks Basavanagouda