Hi Technical team, After the long periods of search i found that STM8L series microcontrollers are suitable for consuming low power.But i found only STM8L152C6T6 Discovery board on internet. May i know what are the other development or discovery boar...
Hi Technical team, I know that STM8L152C6T6 chip is having UART option.I have STM8L152C6T6 Discovery board and checked its schematic also but i could not find out UART-TX & UART-RX pins.Pls help me to check that UART transmit and receive functional...
Hi Technical team, UART2 is always sending garbage value rather required(correct) value. Hardware used : STM8S discovery with 5V IDE used : IAR The below shows the code , // STM8S105 discovery #include "stdio.h" #in...
Posted on February 19, 2016 at 14:35Hi all, I need to know, BlueNRG firmware version which is flashed in my BlueNRG chip without using BlueNRG GUI window. What are the possibilities to get this ? Can i get this from SPI ? or give me prope...
Posted on February 04, 2016 at 13:55Hi all, In BlueNRG chat application, i can able to transfer and receive data if the packet size was 20 or below. When i change the packet size more than 20 bytes , communication doesn't started. But i n...
Hi, Thanks for your responseI have modified code as per your suggestion, it was compiled successfully in IAR but still output is printing garbage values only in terminal.I have used two type of terminal software to test this 1. TeraTerm 2. Rea...
Hi, Thanks for your replyPlease find the below response for your reply1.As putchar is not taking in IAR , i renamed that function name as "send" and compiled successfully in IAR IDE .2. As main is only having printf, it is not printing anything on ...
Posted on January 13, 2016 at 10:03Hi , Please tell me the procedure to generate Static Random address for BlueNRG. Because i also tried to read board address, but all the board gives same address.
Posted on December 10, 2015 at 07:18Hi, Thank you... Problem Solved First i tried IAR compiler and ST link debugger for flashing DFU image file (not solved, that was my 2nd post) After that i tried ST link utility exe (downloader...
Posted on December 08, 2015 at 07:17 Hi Marchese.Graziella, I tried that by using STlink but it is also not working. I have attached the log window which shows some warning
________________
Attachments : dfu.png : https://st--c.eu1...