Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF01SA Do not list open networks

Posted on February 23, 2017 at 22:04Hello I'm using SPWF01SA wifi module. When I do AT+S.SCAN all the available networks around are listed except the open ones. I can see every password protected networks (WPA2) but the open networks are not even se...

sergetr by Associate II
  • 879 Views
  • 1 replies
  • 0 kudos

BLE File Transfer

Posted on February 23, 2017 at 14:49Hi everyone, I want to implement a very simple file transfer via BLE from my SensorTile to a remote device.I need to edit the BlueMicrosystem2 V2.2.0 firmware in order to add a new characteristic: such a character...

SPWF01SA and WPA Enterprise authentication

Posted on February 22, 2017 at 17:17Hi, i began evaluating the SPWF01SA module, and i managed to make it work with most of the WPA2- personal authenticated networks. I was wondering though, is it possible for the module to join a WPA-enterprise auth...

wifi_opr_rate_mask

Posted on February 22, 2017 at 11:29Hi,We use SPWF01SC module in customer product. Device will be used in complex WiFi environment.We tried to test WLAN connectivity in 802.11b, g and n setups in order to determine which one will better serve our ne...

Grigori by Associate II
  • 999 Views
  • 2 replies
  • 0 kudos

Spirit SP1ML internal schematic

Posted on January 10, 2016 at 15:06I'm developing a custom firmware for SP1ML but I miss important info regarding connections between the STM32L151RB and the SPIRIT chips. Analysing the firmware loaded on the SP1ML, I understood that:    PA5     ---...