cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting SPWF01S using WPS

pontus2
Associate II
Posted on June 27, 2016 at 13:52

Hello!

Is there a way to connect to an existing AP without hardcoding the SSID, login credentials etc? For example, using WPS. In the AT command spec there is a Table defining some errors where number 21 has the message ''Cannot use GPIO7. Reserved for WPS

 

feature''  but the meaning is set to ''!!!!Ignore!!!!''. Is this an upcoming feature? Or is there any other way to be able to connect to an arbitrary local AP?

Regards,

Pontus
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gerardo GALLUCCI
ST Employee
Posted on July 04, 2016 at 11:21

WPS is not part of SPWF01Sx features. You can use miniAP firstset webpage, and fill target AP credentials