Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Mystery chip SP01 P511

Posted on March 03, 2017 at 23:47I have chip on which there's (probably) SP01 P511 (Picture attached). It was manufactured by ST. Probably it's W-MBUS module (or RF in general). I cannot find it anywhere. Do you have datasheet for it?#rf-receiver-tr...

Problem application bluetooth don't send character and display Error 507 on app with mbed program

Posted on February 27, 2017 at 15:26Hello,I've got a problem with this program I can't send a character with an application btle 'Error 507' Displayed on the app.What's the problem?/* mbed Microcontroller Library Copyright (c) 2006-2015 ARM Limited...

SWPF01 - About SSI tags dataflow

Posted on March 01, 2017 at 18:02Hello,I have some trouble trying to use SSI tags in custom html page. I can't manage to make it usable...Let me explain a bit:(All the following is hardcoded)First, I create a file :AT+S.FSC=/test.shtml,100\r?And put...

Sensortile BlueNRG-MS Firmware

Posted on February 28, 2017 at 16:22Hi,I am working on Sensortile kit with the BlueNRG-MS radio.As per ST document PM0237 section 3.3, pg 55/99, following commands are used to add custom service to BLE device : //Add the service with service_uuid 12...

RADS1 by Associate II
  • 717 Views
  • 0 replies
  • 0 kudos

Sensortile BlueNRG-MS Custom Service ACI

Posted on February 28, 2017 at 16:18Hi,I am working on Sensortile kit with the BlueNRG-MS radio.As per ST document PM0237 section 3.3, pg 55/99, following commands are used to add custom service to BLE device : //Add the service with service_uuid 12...

RADS1 by Associate II
  • 782 Views
  • 0 replies
  • 0 kudos

BlueNRG won't enter DFU mode

Posted on February 23, 2017 at 14:35I have a BlueNRG IDB005V1D board which is connected to its motherboard. I am trying to install firmware onto the STM32L151RBT6 uC on the motherboard but when I am prompted to enter DFU mode there is no LED flashin...

daithi62 by Associate II
  • 751 Views
  • 1 replies
  • 0 kudos

Resolved! How to compute the best connection interval?

Posted on February 18, 2017 at 00:48Hi,My BlueNRG-MS, running 7.2c, acts both as a central and a peripheral (mode 4). How should I select the advertizing min and max intervals for the peripheral as well as the connection min and max intervals for th...

hardware by Associate II
  • 1297 Views
  • 2 replies
  • 0 kudos

Resolved! BlueNRG-MS write to remote characteristic

Posted on February 23, 2017 at 16:21I try to write to a characteristic on a remote device, BlueNRG-MS works as peripheral client. I call aci_gatt_write_charac_value() and it returns SUCCESS. But then EVT_BLUE_GATT_PROCEDURE_COMPLETE comes and it is ...

grzegorz by Associate III
  • 1373 Views
  • 2 replies
  • 0 kudos