cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG won't enter DFU mode

daithi62
Associate II
Posted on February 23, 2017 at 14:35

I have a BlueNRG IDB005V1D board which is connected to its motherboard. I am trying to install firmware onto the STM32L151RBT6 uC on the motherboard but when I am prompted to enter DFU mode there is no LED flashing orange, and and the attempted flash fails.

I tried using the STM32 ST-LINK Utility also to load the DFU_Bootlader.hex but this says that there was no ST-Link device detected. The ST-Link connector that I use does work on another board.

Are there any suggestions as to how I can flash the uC? 

Thank you ,

cod

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
daithi62
Associate II
Posted on February 27, 2017 at 12:37

I managed to sort this issue using the process detailed in the following link;

http://www.keil.com/support/man/docs/uv4/uv4_fl_hexdownload.htm