cancel
Showing results for 
Search instead for 
Did you mean: 

BLE File Transfer

Andrea De Lorenzo
Associate
Posted on February 23, 2017 at 14:49

Hi everyone, I want to implement a very simple file transfer via BLE from my SensorTile to a remote device.

I need to edit the BlueMicrosystem2 V2.2.0 firmware in order to add a new characteristic: such a 

characteristic should read a file from the SD card and send them from the SensorTile to the remote device (a kind of reverse FOTA).

Reading the file is not a problem, but I have no idea where to start from for developing the service which provides this file upload 

characteristic.

Can you point out a code snippet or where, in the firmware code, there is a similar GATT service that may be adapted easily to me needs. 

Tnx!

Andrea

#ble #bluenrg #sensor-tile
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0