Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[bug] Wrong sizeof in SimpleBlueNRG_HCI

Posted on December 07, 2017 at 15:43In the files STM32CubeExpansion_BLE1_V3.2.0\Middlewares\ST\STM32_BlueNRG\SimpleBlueNRG_HCI\hci\controller\bluenrg_hal_aci.cbluenrg_gap_aci.cWe can see some Osal_MemCpy with wrong sizeof. Ex in bluenrg_gap_aci.c:tB...

nicolas b by Associate III
  • 707 Views
  • 1 replies
  • 0 kudos

Questions on the S2-LP transceiver

Posted on June 20, 2017 at 11:26Hello,we are designing an RF interface for the ISM 868-870 MHz band.We are attracted to the S2-LP transceiver mainly because it drains only 10 mA at 10 dBm RF output powerI got a couple of questions about the S2-LP tr...

S2-LP Sigfox Application

Posted on December 15, 2017 at 10:05Hello,I am trying to develop a Sigfox application with the S2-LP transceiver.I bought the STEVAL-FKI868V1 evaluation kit and I downloaded the STSW-S2LP-SFX-DK software.Everything works well with the kit, but now I...

L J by Associate
  • 841 Views
  • 0 replies
  • 0 kudos

First Time Connection SPWF04SA - Faild ,please help

Posted on December 12, 2017 at 22:52Hello running the example code  : WIFI_Example_Client_Socketusing SPWF04SAalso the server program in the st utility ip 10.0.0.1 (checked with external socket.exe and worekd)but the WIFI_Example_Client_Socket  moo ...

maor by Associate III
  • 745 Views
  • 1 replies
  • 0 kudos

SPWF04SA ST COMMAND PDF ?

Posted on December 12, 2017 at 22:59Hello ,we would like to use the wi fi  SPWF04SA as stand aloneusing in uart1/ where can i find short simple l example code script ..setup sid ,key.....open socket ip/port send hellow word , and close socket ?2.whe...

maor by Associate III
  • 1049 Views
  • 1 replies
  • 0 kudos

SPWF04Sx FW Source

Posted on December 12, 2017 at 14:19Is $SUBJECT available ?Given the absence of detailed SPI protocol descriptions (and the problems I face), I'd love to read the source.I'd like to implement a custom RTOS task on the module. I don't need microphyth...